|
||||||||||||||||
Automotive Night VisionAutomotive Night Vision allows you to see in total darkness. With the PathFindIR Automotive Night Vision System, you can see road hazards like animals, pedestrians and disabled vehicles long before you can see them with headlights. Thermal Imaging, Night Vision and Infrared Cameras For Law EnforcementFLIR Systems is the world's leading supplier of thermal imaging systems for law enforcement missions. We offer products to match any law enforcement mission whether it be in the air, on the water, or on the ground. Many different models and options are available to match your specific mission and budget. Thermal Imaging, Night Vision and Infrared Cameras For SecurityA thermal imager is a camera which is capable of detecting extremely small temperature differences. These temperature differences can be converted into a real-time video image. Displayed on a monitor, this video image is extremely suited for night vision applications. Unlike other night vision systems that require low amounts of light to generate an image, a thermal imager needs no light at all. This makes it the perfect tool to see in absolute darkness, to see during the darkest night. Thermal Imaging, Night Vision and Infrared Cameras For MaritimeThermal imagers are very effective in maritime environments. They can detect objects floating in the water which may damage a vessel, or even worse, sink it. Other vessels, shipping lane traffic, buoys, bridges, ... it is all seamlessly detected by thermal imaging. Even objects which can not be detected by a radar system such as sail boats, wooden boats, floating debris, ... become clearly visible when you are using a thermal imager. Thermal Imaging, Night Vision and Infrared Cameras Cores and ComponentsFLIR offers a full line of uncooled and cooled infrared sensors and component products under the ''Core by Indigo'' brand. FLIR's volume detector fabrication capability, ROIC development, OEM packaging and program management can provide you with the highest quality sensors at the lowest cost, and supported by some of the most respected experts in the industry. Thermal Imaging, Night Vision and Infrared Cameras For for AviationFLIR's EVS3™ is a low cost thermal imager for use as a pilot's night vision enhancement. It aids pilots by enhancing the ability to see terrain and other aircraft at long ranges, even in total darkness, light fog, dust and smoke. The EVS3 is designed for integration with existing multi-function displays, with a simple “power in and standard video out” interface. It includes FLIR's patented Dynamic Digital Detail Enhancement (DDE) assuring excellent image quality regardless of scene dynamics, revealing scene detail missed by more expensive competitive systems. A choice of three lens options is available to accommodate various flight profiles with a wide, medium and narrow field of view. |
||||||||||||||||